LPC5528 USB1 as full speed device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC5528 USB1 as full speed device

ソリューションへジャンプ
1,770件の閲覧回数
tks11111
Contributor II

Hi All, 

I found a thread that discussed how to use USB1 as a full-speed device.

LPC55S6x USB1 as full speed device - NXP Community

Do I need to change the clock setting if I set the bit 21 of the USB1 device command/status register (DEVCMDSTAT) to 1?
Also, do I need to add any other speed configuration?

Appreciate any help.

Thanks.

 

BR,

Peter 

ラベル(2)
0 件の賞賛
返信
1 解決策
1,714件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI tks11111,

There is no need setting clock. 

To set LPC5528 USB1 as full speed device, setting Forced FS bit as 1 is enough.

Best Regards,

Jun Zhang

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,715件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI tks11111,

There is no need setting clock. 

To set LPC5528 USB1 as full speed device, setting Forced FS bit as 1 is enough.

Best Regards,

Jun Zhang

0 件の賞賛
返信