LPC5528 USB1 as full speed device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC5528 USB1 as full speed device

Jump to solution
1,765 Views
tks11111
Contributor II

Hi All, 

I found a thread that discussed how to use USB1 as a full-speed device.

LPC55S6x USB1 as full speed device - NXP Community

Do I need to change the clock setting if I set the bit 21 of the USB1 device command/status register (DEVCMDSTAT) to 1?
Also, do I need to add any other speed configuration?

Appreciate any help.

Thanks.

 

BR,

Peter 

Labels (2)
0 Kudos
Reply
1 Solution
1,709 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI tks11111,

There is no need setting clock. 

To set LPC5528 USB1 as full speed device, setting Forced FS bit as 1 is enough.

Best Regards,

Jun Zhang

View solution in original post

0 Kudos
Reply
1 Reply
1,710 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI tks11111,

There is no need setting clock. 

To set LPC5528 USB1 as full speed device, setting Forced FS bit as 1 is enough.

Best Regards,

Jun Zhang

0 Kudos
Reply