LPC5528 Force USB1 as Full speed Device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC5528 Force USB1 as Full speed Device

Jump to solution
2,450 Views
tks11111
Contributor II

Hi,

I'm using the LPC5528 to run a project, and I need to support both high speed USB and full speed USB by using USB1. I saw there is a Forced FS bit in USB1->DEVCMDSTAT that might be able to deal with it.

However, as I know, there are some differences between high speed USB and full speed USB such as the clock and the descriptor.

My questions are:

1. Do we need to do any configuration after setting the Forced FS bit to 1 if I want to force USB1 as a USB full speed device. 

2. Do we need to adjust any clock setting for it?

3. Is there any sample code that can be referenced? (toggle USB high speed and USB full speed in USB1)

 

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
2,423 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @tks11111 

 

Setting the Force FS bit to 1 is the only thing that is required.

Nothing else needs to be done. Clocks and other items are automatically configured by the HW in the correct mode.

 

 

BR

Alice

View solution in original post

0 Kudos
Reply
2 Replies
2,424 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @tks11111 

 

Setting the Force FS bit to 1 is the only thing that is required.

Nothing else needs to be done. Clocks and other items are automatically configured by the HW in the correct mode.

 

 

BR

Alice

0 Kudos
Reply
2,412 Views
tks11111
Contributor II

Hi Alice,

Thanks for the quick reply.

I had a quick question. If I want to toggle the USB1 between High Speed and Full Speed, I need to

call NVIC_SystemReset() and then toggle the Forced FS bit in the beginning, right?

0 Kudos
Reply