LPC5528 CFPA and CMPA programming process

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC5528 CFPA and CMPA programming process

6,837 Views
gary_yang
Contributor II

Hi Sir:

We are a third-party programmer manufacturer.

Currently developing LPC5528 CFPA and CMPA programming process, using ISP Uart.

But at the beginning of sending (0x5A 0xA6) (baud rates 115200), the IC did not respond, it seems that the Uart communication failed

擷取5.JPG

 Our schematic is below, do you have any suggestions?

擷取2.JPG

 

0 Kudos
Reply
5 Replies

6,691 Views
gary_yang
Contributor II

Hi Sir:

 

Our circuit can use SWD to programing Flash,but use Uart to send data (0x5A 0xA6), IC does not respond.

Generally speaking, after the power on,Uart sends data (0x5A 0xA6), will the IC respond? Is there any other process required?

 

Thanks

0 Kudos
Reply

6,679 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, the LPC5528 does not have any reference for a power sequence or timing. 

  • After the bootloader detects the Ping packet (0x5A 0xA6) on UARTn_RX, the bootloader firmware executes the autobaud sequence.

Could you confirm if you have the possibility to check if the signal goes to the MCU in an oscilloscope? to confirm if the 0x5A has integrity.

Best regards,
Pavel

 

0 Kudos
Reply

6,819 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, I reviewed your information and I recommend reviewing the chapter 6.1 Pin description, I think the method to enter in ISP is missing.

Pavel_Hernandez_0-1685046894154.png

From User Manual.

Pavel_Hernandez_1-1685047103143.png

Let me know if you have more doubts.

Best regards,
Pavel

 

0 Kudos
Reply

6,787 Views
gary_yang
Contributor II
Hi Sir:
ISP0 (PIO0_5 pin) has been pulled low, but send (0x5A 0xA6) (baud rate 115200), IC still does not respond
Is there any other setting required to use ISP mode (UART)?
0 Kudos
Reply

6,748 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I review your schematic, I recommend reviewing the schematic for the EVK if you want to use the USB and DCDC, in another way I recommend reviewing this app note Hardware Design Guidelines for LPC55(S)xx Microcontrollers (nxp.com). 

Pavel_Hernandez_0-1685393669485.png

The logic state determines the boot source.

Pavel_Hernandez_1-1685393979290.png

Pavel_Hernandez_3-1685394001293.png

Best regards,
Pavel

 

0 Kudos
Reply