LPC551x newbie questions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC551x newbie questions

1,015 次查看
alanto
Contributor I

Hi,

On cursory inspection, it looks like the M33 is an M4 but without the DSP and with more security features, is that approximately correct?

Is there an encrypted bootloader app/app note/example for the LPC551x?

Is there CMSIS?

Is Keil supported?

标签 (1)
0 项奖励
回复
1 回复

963 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Alan

On the LPC55S1x/LPC551x, the Cortex-M33 is augmented with hardware co-processors providing accelerated support for additional DSP algorithms.
The Arm Cortex M33 provides a security foundation, offering isolation to protect valuable IP and data with TrustZone technology. It simplifies the design and software development of digital signal control systems with the integrated digital signal processing (DSP) instructions

LPC55Sxx supports secure boot. please make sure you use LPC55S1x

https://www.nxp.com/docs/en/application-note/AN12283.pdf 

CMSIS and Keil are supported.

Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复