LPC5514JBD64E Use for WS2812.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC5514JBD64E Use for WS2812.

56件の閲覧回数
Kishore02
Contributor I

Hi, Is LPC5514JBD64E suitable for working with WS2812 for a beginner. If yes Where Can I get The Code and other Details. 

Thank you.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

42件の閲覧回数
carlos_o
NXP TechSupport
NXP TechSupport

hi @Kishore02 

Thank you for your post!

There is not information about the implementation of WS2812 for the LPC551x, you could use the Programmable Logic Unit to do it, in another devices there are example using the FlexIO modules like in application code hub for the MCXA366: https://mcuxpresso.nxp.com/appcodehub?search=an-emulating-ws2812-bus-with-flexio-on-mcx366 

Also, there is a post of a colleague that implement it for a Kinetis board: NXP FlexIO Generator for the WS2812B LED Stripe Protocol

Hope this information help as a reference 

0 件の賞賛
返信