LPC550x code read protection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC550x code read protection

1,922件の閲覧回数
johanleroy
Contributor I

Hi,

On previous NXP MCU's there was a CRP to configure code read protection. How can we enable code read protection on the LPC550x MCU.

 

Thanks in advance

Kind regards

Johan Leroy

ラベル(2)
0 件の賞賛
返信
1 返信

1,906件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @johanleroy 

I hope that you are doing well!

All of the LPC55 MCUs provide  features to disable ISP entry and debug access , even the ones that do not have an S ( LPC55S security modules such as PRINCE , secure boot etc. ). This is done by setting dedicated bits on the CMPA and CFPA areas  protected flash region or PFR. Refer to SOCU_PIN and SOCU_DFLT on the user manual

The PFR can be programmed from the application (using API) or using tools such as the MCUXpresso secure provisioning tool , elftosb gui, or by  directly writing CMPA and CFPA using bl-host. 

Those settings might be confusing at first glance and if there is any improper setting into the PFR you might brick your chip. If you disable ISP and debug access you won't be able to recover the MCU externally.

Let me know if  you have any other question

Diego.

0 件の賞賛
返信