LPC5502 SWD not detected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC5502 SWD not detected

Jump to solution
12,565 Views
christianlees
Contributor III

Hello,

I know a similar question has been asked and I have gone through the solution will no luck.

I cannot get the device to be detected on the SWD interface.  I'm using s Segger JLink EDU.  The board didn't have the XTAL32M_P or XTAL32K_P pins ties to ground so I wired them in as with the pull up on PIO0_5.  The attached schematic shows the current arrangement.

I am seeing 1.052V on C39 as expected.

Could be a power issue, any help is appreciated.

Thanks

Christian

Labels (1)
0 Kudos
Reply
1 Solution
12,412 Views
christianlees
Contributor III

I got it to work by getting a newer debugger.  If you are using a Segger Jlink it needs to be later then V8.0 hardware

View solution in original post

0 Kudos
Reply
8 Replies
12,413 Views
christianlees
Contributor III

I got it to work by getting a newer debugger.  If you are using a Segger Jlink it needs to be later then V8.0 hardware

0 Kudos
Reply
12,546 Views
christianlees
Contributor III

I took a capture of the a SWD transaction, I don't know the protocol but it looks like the ACK works and it responds.

If I try it from the command line this is the output

Type "connect" to establish a target connection, '?' for help
J-Link>connect LPC5502
Please specify device / core. <Default>: LPC5502
Type '?' for selection dialog
Device>
Please specify target interface:
J) JTAG (Default)
S) SWD
T) cJTAG
TIF>s
Specify target interface speed [kHz]. <Default>: 4000 kHz
Speed>
Device "LPC5502" selected.


Connecting to target via SWD
ConfigTargetSettings() start
Disabling flash programming optimizations: Compare, SkipBlankDataOnProg
ConfigTargetSettings() end
InitTarget() start
ERROR: Wrong DM-AP IDCODE detected: 0x00000000
InitTarget() end
ConfigTargetSettings() start
Disabling flash programming optimizations: Compare, SkipBlankDataOnProg
ConfigTargetSettings() end
InitTarget() start
ERROR: Wrong DM-AP IDCODE detected: 0x00000000
InitTarget() end
ConfigTargetSettings() start
Disabling flash programming optimizations: Compare, SkipBlankDataOnProg
ConfigTargetSettings() end
InitTarget() start
ERROR: Wrong DM-AP IDCODE detected: 0x00000000
InitTarget() end
ConfigTargetSettings() start
Disabling flash programming optimizations: Compare, SkipBlankDataOnProg
ConfigTargetSettings() end
InitTarget() start
ERROR: Wrong DM-AP IDCODE detected: 0x00000000
InitTarget() end
Cannot connect to target.
J-Link>

 

0 Kudos
Reply
12,533 Views
christianlees
Contributor III

I've done some reading and it looks like the IDCODE for a Cortex-M33 should be 0xBA04 yet mine is returning 0xBA02, this is clear in the previous captured screen shot. I have both tested from the IDE as well as the JLink console program.

J-Link>readdp 0
Reading DP register 0 = 0x6BA02477 (0 read repetitions needed)

Could this be the issue?  Could it be a damaged MCU?

0 Kudos
Reply
12,555 Views
christianlees
Contributor III

I had already put a pull up on SWD and a pull down on SCK on my programming breakout board.  Putting on the PCB containing the LPC5502 will be difficult.  Is the SWO pin actually required?  It hasn't been on any of my other boards where I have used the same programming break out board.

0 Kudos
Reply
12,551 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

If you don't need SWO trace. SWO pin is not needed.

0 Kudos
Reply
12,560 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI christianlees

I suggest you referring this article to check your SWD debug interface design.

https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Design-Considerations-for-Debug/m-p/469565

 

Hope this helps,

Jun Zhang

0 Kudos
Reply
12,467 Views
christianlees
Contributor III

I've changed the MCU, could only get LPC5506 quickly.  Same issue.

Interestingly if I try to debug the incorrect project, one based on an LPC802 then it manages to read the IDCODE and flag it as the incorrect MCU but when I debug the correct project it returns zeros even though the logic analyser says differently.

Sounds like a software issue to me?

Is it a lack of support for the J-Link EDU?

0 Kudos
Reply
12,460 Views
converse
Senior Contributor V

It sounds like you have a problem with your debug circuit. Almost certainly not a software problem. 

0 Kudos
Reply