LPC5500 with DSP accelerator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC5500 with DSP accelerator

4,613件の閲覧回数
arimendes
Contributor III

Hi,

I'm very excited about the  announcement of the new LPC5500 family.

I'm especially curious about the DSP accelerator. Is it accessed as extension instruction set? Or is it a coprocessor? Or is it a peripheral?

Will LPC5500 microcontrollers be for IoT only? Or will be there Industrial applications chips, like Motor control and digital power conversion?

 Ari.

ラベル(2)
0 件の賞賛
返信
4 返答(返信)

3,919件の閲覧回数
arimendes
Contributor III

Hi,

  I found more information about the new LPC5500 coprocessor:

  Named PowerQuad.

  Is it using floating point or fixed point calculations? 

  Anyway, based on the figure, the performance gain are impressive.

   

0 件の賞賛
返信

3,919件の閲覧回数
soledad
NXP Employee
NXP Employee

This family is oriented for Industrial and IoT applications.

Single- or Dual-core Cortex-M33 with integrated DC-DC delivers industry-leading performance at a fraction of power budget, of up to 90 CoreMarks™/mA. The high density of on-chip memory, up to 640KB flash and 320KB SRAM, enables efficient execution of complex edge applications. Further, NXP's autonomous, programmable logic unit for offloading and execution of user-defined tasks delivers enhanced real-time parallelism. For more information about the LPC5500 series, click here.

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

0 件の賞賛
返信

3,919件の閲覧回数
arimendes
Contributor III

Hi Sol,

 Can you tell us when the LPC5500 documentation will be available? 

  

In my opinion, the LPC5xxx analog and digital peripheral sets are too weak for a dual core 100MHZ cortex-m33 with co-processor and 40nm technology.
NXP should had done it based on the much better kinetis KV5x and K80 peripheral set.

0 件の賞賛
返信

3,919件の閲覧回数
leecoakley
Contributor III

Sounds like they are using the coprocessor interface of the M33.  That's good - like with the FPU, you can move 64 bits per cycle across it.  Much better than the peripheral bus.

I'm curious what kind of operations it accelerates too. The DSP functions in the M33 are pretty decent, the same as the Cortex M4.  I'm guessing it widens the number of multiplies per cycle, maybe does fast matrix multiplies.

0 件の賞賛
返信