LPC55 sprintf float values

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55 sprintf float values

449 次查看
SvenAsbach
Contributor II

Hi community,
I am trying to setup sprintf to print float numbers to string.
I tried everything I found, changed libraries, but nothing brought a success.
Either I get not the right result or I get an hardfault when trying to print negative float values.

Actual processor LPC5506
Floating point unit FPv5-SP-D16 Hard ABI set
current library setting Redlib semihost
I am using UART0 to print

PreProcessor settings
CPU_LPC5506JBD64
CPU_LPC5506JBD64_cm33
SDK_OS_BAREMETAL
SDK_DEBUGCONSOLE=2
SERIAL_PORT_TYPE_UART=1
PRINTF_FLOAT_ENABLE=1
SCANF_FLOAT_ENABLE=1
PRINTF_ADVANCED_ENABLE=1
SCANF_ADVANCED_ENABLE=1
__MCUXPRESSO
__USE_CMSIS
DEBUG
DISABLEFLOAT16
__REDLIB__

trying this code

float P_Value = 3.123456f;

float I_Value = 123.4567f;

float D_Value = 0.654321f;

sprintf(g_txBuffer, "rpm = %d, P_Value = %f, I_Value = %f, D_Value = %f \r", rpm_ist, P_Value, I_Value, D_Value);

no warnings or errors

And the result is
rpm = 206, P_Value = -0.000000, I_Value = -0.000000, D_Value = -0.000000 <CR>

 

Is there a way to get sprintf to print the right values including negative values or do I have to write my own converter?
What I do not see?

 

Thanks in advance

 

标签 (2)
标记 (3)
0 项奖励
回复
6 回复数

230 次查看
SvenAsbach
Contributor II

Stdio.h is included and used.

Where can I check in an existing project that the right printf version is used or where do I change it?
My preprocessor settings I have already send to you.

CR_INTEGER_PRINTF is not used in the build


Build is done with


arm-none-eabi-gcc -DCPU_LPC5506JBD64 -DCPU_LPC5506JBD64_cm33 -DSDK_OS_BAREMETAL -DSDK_DEBUGCONSOLE=2 -DSERIAL_PORT_TYPE_UART=1 -DPRINTF_FLOAT_ENABLE=1 -DSCANF_FLOAT_ENABLE=1 -DPRINTF_ADVANCED_ENABLE=1 -DSCANF_ADVANCED_ENABLE=1 -D__MCUXPRESSO -D__USE_CMSIS -DDEBUG -DDISABLEFLOAT16 -D__REDLIB__ xxxxx -O0 -fno-common -g3 -gdwarf-4 -Wall -c -ffunction-sections -fdata-sections -fno-builtin -fmerge-constants -fmacro-prefix-map="../CMSIS/DSP/Source/BayesFunctions/"= -mcpu=cortex-m33 -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -D__REDLIB__ -fstack-usage -specs=redlib.specs -MMD -MP

0 项奖励
回复

135 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @SvenAsbach 

Please make sure the project defined symbols and floating point set as below:

ZhangJennie_1-1757489388300.png

ZhangJennie_2-1757489476615.png

 

Hope this helps,

Jun Zhang

 

 

 

0 项奖励
回复

423 次查看
SvenAsbach
Contributor II

Thanks for the fast answer, but this does not help.
All what you are proposing is already set and tried, but no success.
Compiler uses this

arm-none-eabi-gcc -DCPU_LPC5506JBD64 -DCPU_LPC5506JBD64_cm33 -DSDK_OS_BAREMETAL -DSDK_DEBUGCONSOLE=2 -DSERIAL_PORT_TYPE_UART=1 -DPRINTF_FLOAT_ENABLE=1 -DSCANF_FLOAT_ENABLE=1 -DPRINTF_ADVANCED_ENABLE=1 -DSCANF_ADVANCED_ENABLE=1 -D__MCUXPRESSO -D__USE_CMSIS -DDEBUG -DDISABLEFLOAT16 -D__REDLIB__ -I"D:\Software\FC5706P_workspace\FC5706P101B001\drivers" -I"D:\Software\FC5706P_workspace\FC5706P101B001\device" -I"D:\Software\FC5706P_workspace\FC5706P101B001\component\serial_manager" -I"D:\Software\FC5706P_workspace\FC5706P101B001\utilities" -I"D:\Software\FC5706P_workspace\FC5706P101B001\component\uart" -I"D:\Software\FC5706P_workspace\FC5706P101B001\CMSIS" -I"D:\Software\FC5706P_workspace\FC5706P101B001\component\lists" -I"D:\Software\FC5706P_workspace\FC5706P101B001\CMSIS_driver\Include" -I"D:\Software\FC5706P_workspace\FC5706P101B001\CMSIS\DSP\Include" -I"D:\Software\FC5706P_workspace\FC5706P101B001\CMSIS\DSP\PrivateInclude" -I"D:\Software\FC5706P_workspace\FC5706P101B001\CMSIS\DSP\Source\DistanceFunctions" -I"D:\Software\FC5706P_workspace\FC5706P101B001\CMSIS\NN\Include" -I"D:\Software\FC5706P_workspace\FC5706P101B001\board" -I"D:\Software\FC5706P_workspace\FC5706P101B001\source" -O0 -fno-common -g3 -gdwarf-4 -Wall -c -ffunction-sections -fdata-sections -fno-builtin -fmerge-constants -fmacro-prefix-map="../CMSIS/DSP/Source/BasicMathFunctions/"= -mcpu=cortex-m33 -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -D__REDLIB__ -fstack-usage -specs=redlib.specs -MMD -MP -MF"CMSIS/DSP/Source/BasicMathFunctions/BasicMathFunctionsF16.d" -MT"CMSIS/DSP/Source/BasicMathFunctions/BasicMathFunctionsF16.o" -MT"CMSIS/DSP/Source/BasicMathFunctions/BasicMathFunctionsF16.d" -o "CMSIS/DSP/Source/BasicMathFunctions/BasicMathFunctionsF16.o" "../CMSIS/DSP/Source/BasicMathFunctions/BasicMathFunctionsF16.c"

0 项奖励
回复

304 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @SvenAsbach 

Did you include "stdio.h"? We need to make sure we have this header file included.

I just tested sprintf with your code, there is no issue on my side. See attached video. 

Please also make sure you use floating point version of printf.

ZhangJennie_0-1756713922369.png

Can you please checking your issue with refering my screenshot and testing video?

Best Regards

Jun Zhang 

 

0 项奖励
回复

426 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @SvenAsbach 

If you use SDK demo, please try to enable floating support 

ZhangJennie_1-1756291243616.png

Make sure the defined symbols, printf float is enabled. 

ZhangJennie_2-1756291670584.png

 

Does this work for you?

Best Regards

Jun Zhang

 

 

 

0 项奖励
回复

426 次查看
ErichStyger
Specialist I

Usually the problem is that CR_INTEGER_PRINTF  is still defined in the -D options list.

Make sure you do a full 'clean' of the build an retry.

These are my (working) defines and Linker settings:

__REDLIB__
CPU_LPC55S69JBD100
CPU_LPC55S69JBD100_cm33
CPU_LPC55S69JBD100_cm33_core0
SDK_DEBUGCONSOLE=1
PRINTF_FLOAT_ENABLE=1
SERIAL_PORT_TYPE_UART=1
__MCUXPRESSO
__USE_CMSIS
DEBUG

ErichStyger_0-1756291258397.png

 

I hope this helps,

Erich