LPC55 On-chip ROM boot via CAN FD?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC55 On-chip ROM boot via CAN FD?

跳至解决方案
1,836 次查看
dav1
Contributor V

The LPC55x series has a nice built-in bootloader in ROM, but I wonder if there are any ways to achieve rom-booting via CAN bus? (CAN-FD to be specific)

It's not listed as a valid boot peripheral in the datasheet, but I'm thinking if we could re-configure or wire the can pins in parallel to standard UART and use a fall-back mechanism so that the "Host" can detect we're not in CAN mode, run the boot-strap process, and then switch back to CAN FD.

 

Thoughts?

0 项奖励
回复
1 解答
1,823 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello dav,

Sorry, no, we have no method to change the code in ROM.

You can development a Secondary bootloader for CAN-FD.

 

Regards,

Alice

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,824 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello dav,

Sorry, no, we have no method to change the code in ROM.

You can development a Secondary bootloader for CAN-FD.

 

Regards,

Alice

0 项奖励
回复