LPC55 On-chip ROM boot via CAN FD?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55 On-chip ROM boot via CAN FD?

ソリューションへジャンプ
1,834件の閲覧回数
dav1
Contributor V

The LPC55x series has a nice built-in bootloader in ROM, but I wonder if there are any ways to achieve rom-booting via CAN bus? (CAN-FD to be specific)

It's not listed as a valid boot peripheral in the datasheet, but I'm thinking if we could re-configure or wire the can pins in parallel to standard UART and use a fall-back mechanism so that the "Host" can detect we're not in CAN mode, run the boot-strap process, and then switch back to CAN FD.

 

Thoughts?

0 件の賞賛
返信
1 解決策
1,821件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello dav,

Sorry, no, we have no method to change the code in ROM.

You can development a Secondary bootloader for CAN-FD.

 

Regards,

Alice

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,822件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello dav,

Sorry, no, we have no method to change the code in ROM.

You can development a Secondary bootloader for CAN-FD.

 

Regards,

Alice

0 件の賞賛
返信