LPC55 / LPC55S36 ISP over USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55 / LPC55S36 ISP over USB

Jump to solution
2,284 Views
BrKu
Contributor II

Good morning,

https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC55-Don-t-Use-ISP-USB0-for-firmware-up...

states to not use USB for ISP due to clock drift.  Does that apply to the LPC55S36?  I was confused to see it in the forums but not in the datasheets or errata.

Thanks

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,069 Views
BrKu
Contributor II

For posterity - our distributor reported that NXP reported the following:

After discussion with the internal team, the internal team believes our LPC5536's ROM code should support FRO trim by full speed USB SOF frame, then the FRO accuracy can match full-speed USB requirement.

There should be no concern on the FRO accuracy, still, we would recommend you perform the test on your devices to validate if this works correctly on your side.

View solution in original post

0 Kudos
Reply
2 Replies
2,069 Views
BrKu
Contributor II

For posterity - our distributor reported that NXP reported the following:

After discussion with the internal team, the internal team believes our LPC5536's ROM code should support FRO trim by full speed USB SOF frame, then the FRO accuracy can match full-speed USB requirement.

There should be no concern on the FRO accuracy, still, we would recommend you perform the test on your devices to validate if this works correctly on your side.

0 Kudos
Reply
2,118 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hello, 

The information was shared directly to your distributor, please reach out to him for the answer. 

Regards, 

Pablo

0 Kudos
Reply