LPC54xxx atol,atoi,strtol Redlib maximum input

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54xxx atol,atoi,strtol Redlib maximum input

ソリューションへジャンプ
3,396件の閲覧回数
kiryat8
Contributor III

I need to parse a decimal string representation of an unsigned 4 byte integer or long.

In my debugger I can see that when the 4 byte value string is 2943834865,

I get a result of 2147483647 (0x7fffffff) from atol,atoi and strtol .

    fileChecksum = atol(Ptr2);
    fileChecksum = strtol(Ptr2,&Ptr1,10);

The debugger:

Ptr2 -> Details:0x20002bd5 <g_bufferRead+13> "2943834865"

Name : fileChecksum
    Details:2147483647
    Default:2147483647
    Decimal:2147483647
    Hex:0x7fffffff
    Binary:1111111111111111111111111111111
    Octal:017777777777

I am guessing that this is because of an overflow from the signed value.

The fileChecksum I defined uint32_t and then as uint64_t with the same result.

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
3,258件の閲覧回数
kiryat8
Contributor III

I also tried to enter the checksum string in hex format and got the same results 0x7fffffff

Today the checksum string was checksum=2939504859=0xAF3548DB.

I tried to enter "AF3548DB" with the strtol function set at base 16.

fileChecksum = strtol(Ptr2,&Ptr1,16);

There may be a linker or compiler setting.

I may just break the string into two parts but other places in my code I use the atoi,atol functions andthe problem may not have yet surfaced.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,258件の閲覧回数
converse
Senior Contributor V

Why not use strtoul? This converts to unsigned long.

3,258件の閲覧回数
kiryat8
Contributor III

Thank you. Of course strtoul is what I was looking for. It works without problem. It makes sense to have strtoul and also strtol which I tried previously, but when you are used to the automatic conversion between signed and unsigned stuff in C, I did not think of it.

The no unsigned integers in Java is just crazy.

Thanks

0 件の賞賛
返信
3,258件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

this function for example atol is defined as:

long int atol(const char *nptr);

Here GNU defined long max as 0x7FFFFFFF(2^31-1), so anything larger than that will out put 0x7FFFFFFF.

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
3,258件の閲覧回数
kiryat8
Contributor III

I knew the size of a signed long but never thought they would think to cap results that actually fit into an unsigned long.

I guess I never noticed this and will have to check the places I use atoi & atol.

Thanks

0 件の賞賛
返信
3,259件の閲覧回数
kiryat8
Contributor III

I also tried to enter the checksum string in hex format and got the same results 0x7fffffff

Today the checksum string was checksum=2939504859=0xAF3548DB.

I tried to enter "AF3548DB" with the strtol function set at base 16.

fileChecksum = strtol(Ptr2,&Ptr1,16);

There may be a linker or compiler setting.

I may just break the string into two parts but other places in my code I use the atoi,atol functions andthe problem may not have yet surfaced.

0 件の賞賛
返信