LPC54S0xx Looking for base address of BOOT ROM RSA API

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54S0xx Looking for base address of BOOT ROM RSA API

1,887 Views
gtkp
Contributor II

Hi,

I'm reading UM11060, Chapter 45.7 RSA API.

The boot ROM provides APIs to perform RSA2048 signature checking routines in
application code.

It goes on to show a table of functions with their offset.  Offset to where?  All I can find in the document is that Boot Rom is between 0x0300 0000 and 0x0300 FFFF. 

Applying the offsets to the start of Boot ROM yields a Hard fault for undefined instruction so that is clearly not the correct base address.  The document does mention that the ROM driver table is at 0x300 0200 and offsets are given for the USB, OTP, AES, RNG but not for the RSA API.

 

Where is a complete document of the ROM driver table for #LPC54S0xx ?

0 Kudos
Reply
3 Replies

1,841 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @gtkp 

I have escalate this issue to DOC and SDK team, they still working on it.

And the latest reply is there is no RSA API in BOOT ROM code.

 

 

BR

Alice

0 Kudos
Reply

1,868 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @gtkp 

 

Try to  address 0x0300 023C ?

If still can not work, please tell me.

BR

Alice

0 Kudos
Reply

1,864 Views
gtkp
Contributor II
Hi Alice,

No the address 0x0300 023C also doesn't work.

Regards,
0 Kudos
Reply