LPC54S0xx Looking for base address of BOOT ROM RSA API

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54S0xx Looking for base address of BOOT ROM RSA API

1,862件の閲覧回数
gtkp
Contributor II

Hi,

I'm reading UM11060, Chapter 45.7 RSA API.

The boot ROM provides APIs to perform RSA2048 signature checking routines in
application code.

It goes on to show a table of functions with their offset.  Offset to where?  All I can find in the document is that Boot Rom is between 0x0300 0000 and 0x0300 FFFF. 

Applying the offsets to the start of Boot ROM yields a Hard fault for undefined instruction so that is clearly not the correct base address.  The document does mention that the ROM driver table is at 0x300 0200 and offsets are given for the USB, OTP, AES, RNG but not for the RSA API.

 

Where is a complete document of the ROM driver table for #LPC54S0xx ?

0 件の賞賛
返信
3 返答(返信)

1,816件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @gtkp 

I have escalate this issue to DOC and SDK team, they still working on it.

And the latest reply is there is no RSA API in BOOT ROM code.

 

 

BR

Alice

0 件の賞賛
返信

1,843件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @gtkp 

 

Try to  address 0x0300 023C ?

If still can not work, please tell me.

BR

Alice

0 件の賞賛
返信

1,839件の閲覧回数
gtkp
Contributor II
Hi Alice,

No the address 0x0300 023C also doesn't work.

Regards,
0 件の賞賛
返信