LPC54S018J4M spifi clock speed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54S018J4M spifi clock speed

ソリューションへジャンプ
3,913件の閲覧回数
rex_lam
Contributor IV

The example spifi source code from mcu-boot initializes the spifi clock speed to 24MHz. Is this NXP's recommendation for the spifi clock speed for spifi flash in LPC54S018J4M? I was wondering if a higher clock rate would be safe to use. Please advise.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,833件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

We can refer this table for spifi clock speed setting. The default IMG_BAUDRATE is 0 which means SPIFI clock speed is 24000000. In source code, when set IMG_BAUDRATE as 96000000 or bigger, SPIFI clock speed is 96000000.

ZhangJennie_0-1620618855675.pngZhangJennie_0-1620618855675.png

So if you want to change SPIFI clock with IMG_BAUDRATE, the maximal clock value is 96000000. The limitation is due to ROM code use internal FRO as clock source.

If you want to get higher SPIFI clock, for example 100MHz, an external clock source and PLL configuration are needed. You can configure SPIFI clock source and divider  in source code to get higher SPIFI clock.

 

Have a nice day,

Jun Zhang

 

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
3,897件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi rex_lam

According to Datasheet,

Quad SPI Flash Interface with 1-, 2-, or 4-bit data at rates of up to 52 MB per second.

ZhangJennie_0-1619589633695.pngZhangJennie_0-1619589633695.png

 

 

Have a nice day,

Jun Zhang

 

0 件の賞賛
返信
3,894件の閲覧回数
rex_lam
Contributor IV

Hi Jun,

Thank you for responding. 52MB/s data rate is not the same as the clock frequency, as it could take into account 4-bit data. Could you advise what the highest allowed clock frequency should be for spifi flash?

Rex

0 件の賞賛
返信
3,887件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

According to UM

Transfer rates of up to SPIFI_CLK/2 bytes per second. This is for 4bit data.

According DS, 

Quad SPI Flash Interface with 1-, 2-, or 4-bit data at rates of up to 52 MB per second. the maximal 52MB is for 4bit data

So we can say maximal SPIFI_CLK is 104MHz.

Here is SPIFI clock source

ZhangJennie_0-1619690771148.pngZhangJennie_0-1619690771148.png

 

If you choose internal FRO96,

  for 4bit data, maximal rate is 96/2=48MB, 

  For 1bit data, maximal rate is 96/8=12MB

 

to get 52MB maximal rate, you need use external clock and configure PLL to reach 104M SPIFI_CLK.

 

Have a nice day,

Jun Zhang

 

0 件の賞賛
返信
3,878件の閲覧回数
rex_lam
Contributor IV

Jun,

Thank you for the clarification. Looking at the XIP project examples in LPC54S018J4M's SDK, it looks like all example XIP projects specify a baud rate of 24MHz by not defining IMG_BAUDRATE.

From the UM:

rex_lam_0-1619722545033.pngrex_lam_0-1619722545033.png

From the startup file:

#ifdef IMG_BAUDRATE
.long IMG_BAUDRATE /* (0x1C) image baudrate */
#else
.long 0 /* (0x1C) reserved */
#endif

Is this indicative of some issue if the baudrate were set higher?

Also, is it possible for NXP to use a different flash part within LPC54S018J4M such that a higher baudrate might not work?

Rex

0 件の賞賛
返信
3,847件の閲覧回数
rex_lam
Contributor IV

I haven't received a response to my recent questions. Does anyone know why the example XIP projects use 24MHz rather than a higher clock speed?

0 件の賞賛
返信
3,834件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

We can refer this table for spifi clock speed setting. The default IMG_BAUDRATE is 0 which means SPIFI clock speed is 24000000. In source code, when set IMG_BAUDRATE as 96000000 or bigger, SPIFI clock speed is 96000000.

ZhangJennie_0-1620618855675.pngZhangJennie_0-1620618855675.png

So if you want to change SPIFI clock with IMG_BAUDRATE, the maximal clock value is 96000000. The limitation is due to ROM code use internal FRO as clock source.

If you want to get higher SPIFI clock, for example 100MHz, an external clock source and PLL configuration are needed. You can configure SPIFI clock source and divider  in source code to get higher SPIFI clock.

 

Have a nice day,

Jun Zhang

 

 

 

 

0 件の賞賛
返信