LPC546xx with 1.8V design and USB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC546xx with 1.8V design and USB

2,317件の閲覧回数
RU
Contributor I

I want to start a LPC546xx design with 1.8V - how can i use USB0?

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,307件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

First of all, pls download the data sheet of LPC546xx from the link:

https://www.nxp.com.cn/docs/en/data-sheet/LPC546XX.pdf

As the following screenshot from above data sheet, you can see that

typical voltage of USB1_AVDD3V3,USB1_AVDDTX3V3 pins are 3.3V

The VDD is from 1.71 to 3.6V, but if you use USB, you have to meet the following condition:

For USB full-speed operation only 3.0 - 3.6 V
For USB high-speed operation only 1.71 - 3.6 V

the VDDA is from 1.71 to 3.6V.

 

 

xiangjun_rong_0-1657851775481.png

Hope it can help you

BR

XiangJun Rong

 

0 件の賞賛
返信

2,267件の閲覧回数
RU
Contributor I

Table 12 says for VDD 1.71V .. 3.6V for USB high speed only. According to this, USB would work with 1.8V.

On the other hand, table 21 shows quite contradictory values. Is USB now possible with 1.8V?

RU_0-1659700050452.png

 

0 件の賞賛
返信

2,245件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I think it is correct:

The VDD is from 1.71 to 3.6V, but if you use USB, you have to meet the following condition:

For USB full-speed operation only 3.0 - 3.6 V
For USB high-speed operation only 1.71 - 3.6 V

 

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信