LPC546xx serial number encoding

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC546xx serial number encoding

跳至解决方案
2,345 次查看
klausrenner
Contributor II

There are 32 characters (alpha and numeric) of serial number available to read from the processor. Can any of these characters be ignored? i.e. are some of the characters related to the processor model rather than serial number? We'd like to track devices with less than 32 character numbers if possible, but of course we want to avoid duplicates.

0 项奖励
回复
1 解答
2,253 次查看
soledad
NXP Employee
NXP Employee

Hi,

The Unique Serial Number or UID is a 128-bit value that is unique across parts/families of LPC Microcontrollers, and no two devices/parts will have all the 128 bits same.

Unfortunately, we do not disclose any information regarding the structure of UID and unique/significant bits. If you require less unique bits (e.g. 8, 16, 32 or 64), whatever method you use collisions will be unavoidable.


Have a great day,

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,254 次查看
soledad
NXP Employee
NXP Employee

Hi,

The Unique Serial Number or UID is a 128-bit value that is unique across parts/families of LPC Microcontrollers, and no two devices/parts will have all the 128 bits same.

Unfortunately, we do not disclose any information regarding the structure of UID and unique/significant bits. If you require less unique bits (e.g. 8, 16, 32 or 64), whatever method you use collisions will be unavoidable.


Have a great day,

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,253 次查看
klausrenner
Contributor II

Thank you very much. This is exactly what I wanted to know.

0 项奖励
回复