LPC546xx serial number encoding

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC546xx serial number encoding

ソリューションへジャンプ
2,381件の閲覧回数
klausrenner
Contributor II

There are 32 characters (alpha and numeric) of serial number available to read from the processor. Can any of these characters be ignored? i.e. are some of the characters related to the processor model rather than serial number? We'd like to track devices with less than 32 character numbers if possible, but of course we want to avoid duplicates.

0 件の賞賛
返信
1 解決策
2,289件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

The Unique Serial Number or UID is a 128-bit value that is unique across parts/families of LPC Microcontrollers, and no two devices/parts will have all the 128 bits same.

Unfortunately, we do not disclose any information regarding the structure of UID and unique/significant bits. If you require less unique bits (e.g. 8, 16, 32 or 64), whatever method you use collisions will be unavoidable.


Have a great day,

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,290件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

The Unique Serial Number or UID is a 128-bit value that is unique across parts/families of LPC Microcontrollers, and no two devices/parts will have all the 128 bits same.

Unfortunately, we do not disclose any information regarding the structure of UID and unique/significant bits. If you require less unique bits (e.g. 8, 16, 32 or 64), whatever method you use collisions will be unavoidable.


Have a great day,

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,289件の閲覧回数
klausrenner
Contributor II

Thank you very much. This is exactly what I wanted to know.

0 件の賞賛
返信