LPC546xx: how do you configure USB1 device ctrl to only enumerate as FS device?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC546xx: how do you configure USB1 device ctrl to only enumerate as FS device?

1,167 次查看
belmontbob59
Contributor IV

UM10912 / Table 935 / DEVCMDSTAT shows that USB1 device controller can enumerate at either FS or HS.

DEVCMDSTAT ::[23:22] Speed (01b FS, 10b HS)

However this field is read only. How can I force USB1 to only enumerate at FS ? . i.e. decline high speed handshaking to expose itself as  FS capable device only to the host.

标签 (2)
标记 (1)
0 项奖励
回复
1 回复

999 次查看
soledad
NXP Employee
NXP Employee

Hi,

Please check the updates in the thread OM13092/Keyboard2mouse : how can I force USB1 device ctrl to be FS ? 


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复