LPC546xx USB1_REXT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,249件の閲覧回数
hirai
Contributor I

Hi.

The reference resistor to connect to USB1_REXT in OM13098: LPCXpresso54628 Development Board is 12.1kohm, but datasheet says 12.4kohm/+-1%. Which is correct?

ラベル(1)
1 解決策
2,032件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Maki Hirai,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Actually, please refer to the datasheet when you design.

Hope this is clear.

Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,033件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Maki Hirai,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Actually, please refer to the datasheet when you design.

Hope this is clear.

Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------