LPC546xx: USB1_REXT when USB1 is unused

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC546xx: USB1_REXT when USB1 is unused

2,305件の閲覧回数
giusloq
Contributor III

Should I connect USB1_REXT pin to an external resistor even when USB1 is not used on the board? What happens if UDB1_DM/USB1_DP/USB1_REXT are not connected, while USB1 VDD signals (USB1_AVDDC3V3, USB1_AVDDTX3V3, USB1_VBUS) are tied to VDD?

I found recommended connections of some unused pins in the datasheet, but USB1_REXT is not descripted.

 

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,289件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @giusloq 

You can leave the UBS1_REXT pin unconnected if you are not using USB1 functions. And if you have connected the USB1_VBUS, USB1_AVDDC3V3 and USB1_AVDDTX3V3 to VDD it doesn’t affect the UDB1_DM, USB1_DP and USB1_REXT.

 

B.R.

VaneB

0 件の賞賛
返信

2,282件の閲覧回数
giusloq
Contributor III

You can leave the UBS1_REXT pin unconnected if you are not using USB1 functions. And if you have connected the USB1_VBUS, USB1_AVDDC3V3, USB1_AVDDTX3V3 and USB1_AVSSTX3V3 to VDD it doesn’t affect the UDB1_DM, USB1_DP and USB1_REXT.

Ok, thank you for the answer. However I think you made an error with USB1_AVSSTX3V3: this pin should be tied to VSS, not VDD.