LPC546xx: USB1_REXT when USB1 is unused

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC546xx: USB1_REXT when USB1 is unused

2,323 Views
giusloq
Contributor III

Should I connect USB1_REXT pin to an external resistor even when USB1 is not used on the board? What happens if UDB1_DM/USB1_DP/USB1_REXT are not connected, while USB1 VDD signals (USB1_AVDDC3V3, USB1_AVDDTX3V3, USB1_VBUS) are tied to VDD?

I found recommended connections of some unused pins in the datasheet, but USB1_REXT is not descripted.

 

Labels (2)
0 Kudos
Reply
2 Replies

2,307 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @giusloq 

You can leave the UBS1_REXT pin unconnected if you are not using USB1 functions. And if you have connected the USB1_VBUS, USB1_AVDDC3V3 and USB1_AVDDTX3V3 to VDD it doesn’t affect the UDB1_DM, USB1_DP and USB1_REXT.

 

B.R.

VaneB

0 Kudos
Reply

2,300 Views
giusloq
Contributor III

You can leave the UBS1_REXT pin unconnected if you are not using USB1 functions. And if you have connected the USB1_VBUS, USB1_AVDDC3V3, USB1_AVDDTX3V3 and USB1_AVSSTX3V3 to VDD it doesn’t affect the UDB1_DM, USB1_DP and USB1_REXT.

Ok, thank you for the answer. However I think you made an error with USB1_AVSSTX3V3: this pin should be tied to VSS, not VDD.