I'd like to output a PWM signal from CT4_MAT3 pin. I read a small not on User Manual:
Note: It is recommended to use match channel 3 to set the PWM cycle.
Is it recommended or mandatory, and why?
I tried to use MAT3 for PWM output and MAT0 for PWM cycle, like this:
CTIMER_SetupPwm(CTIMER4,
kCTIMER_Match_0, // pwmPeriodChannel
kCTIMER_Match_3, // matchChannel
50,
10000,
12000000,
0);but at first it didn't work. Then I noticed this instruction in CTIMER_SetupPwm:
reg |= CTIMER_MCR_MR3R_MASK;that says to reset the timer counter on MR3. After replacing with:
reg |= CTIMER_MCR_MR0R_MASK;I was able to generate my PWM output from CT4_MAT3.
Is it ok? Why there's such a limitation?
已解决! 转到解答。
Hello,
Yes, you can .
I think this note is come from old parts, because old products, the match 3 is not routed to output pin, it
can not output PWM, so recommend it as PWM cycle.
While MATCH3 pin out with lpc546xx.
BR
Alice
Hello,
Yes, you can .
I think this note is come from old parts, because old products, the match 3 is not routed to output pin, it
can not output PWM, so recommend it as PWM cycle.
While MATCH3 pin out with lpc546xx.
BR
Alice