LPC546xx Ethernet documentation problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC546xx Ethernet documentation problem

1,583 Views
Anonymous
Deactivated User

Hi,

the documentation for the Ethernet peripheral in UM10912 is not correct.

On page 825 (rev 2.3 - 17 June 2016) the DMA interrupt enable register shows:

  • Bit 6: RIE: When this bit is set with abnormal interrupt summary enable (bit 16 in this register), receive
    interrupt is enabled
  • Bit 15: Normal interrupt summary enable.
    When this bit is set, a normal interrupt is enabled. When this bit is reset, a normal interrupt is
    disabled. This bit enables the following bits:
    DMA channel status register Table 858, bit 0: transmit interrupt
    DMA channel status register Table 858, bit 2: transmit buffer unavailable
    DMA channel status register Table 858, bit 6: receive interrupt
    DMA channel status register Table 858, bit 14: early receive interrupt
  • Bit 31-16: Reserved

Am I correct inassuming that "abnormal interrupt summary enable (bit 16 in this register)" should read "normal interrupt summary enable (bit 15 in this register)"

and am I also correct in assuming that the bits 14 and 15 are sort of masking the complete group of abnormal and normal interrupts so bit 15 should always be 1 for any of the normal interrupts to fire?

Regards,

Rob

Labels (1)
Tags (1)
1 Reply

1,476 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi robjansen‌,

I think you're right, I will inform about this issue. Thanks a lot for your feedback.

Best Regards,

Alexis Andalon