LPC546x USB stack code documentation for example dev_cdc_vcom_bm not found

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC546x USB stack code documentation for example dev_cdc_vcom_bm not found

1,551 次查看
yiningzhang
Contributor I
SDK Name: SDK_2.x_LPCXpresso54608
SDK Version: 2.4.1 (2018-06-18)
Example Name: usb_examples/dev_cdc_vcom_bm
 
Expected Usage:
 
We use LPC54606/54608 to setup virtual com service to Mac / PC, and use Mac / PC serial service to stream data from board. Since there is no actual “serial port” on either side, the speed should be USB 2.0 High-Speed, which is 480Mb/s in bare PHY, not considering communication overheads.
 
In experiments, we do cover the current speed needs, which is 16MB/s.
 
Now we would like to learn more about this code. The top-level entry is:
USB_DeviceCdcAcmSend(s_cdcVcom.cdcAcmHandle, USB_CDC_VCOM_BULK_IN_ENDPOINT, s_currSendBuf, size);
 
which calls:
USB_DeviceSendRequest(cdcAcmHandle->handle, ep, buffer, length);
 
which calls
deviceHandle->controllerInterface->deviceSend(deviceHandle->controllerHandle, endpointAddress,buffer, length);
 
This seems to be the last level we could reach. Is there any documentation on how the bottom-level USB stack is organized or runs? 
标签 (1)
0 项奖励
回复
1 回复

1,414 次查看
soledad
NXP Employee
NXP Employee

Hi, 

Check attached the SDK USB docs.

Have a great day,

Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复