LPC54628 package options

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54628 package options

1,504件の閲覧回数
andyjackson
Contributor III

Is the BGA180 package going to be the only option for this part? We would like the performance boost of the LPC54628, but the QFP208 would an better package for low volume and prototyping as it is more suitable for manual assembly and rework.

Thanks,

Andy

ラベル(3)
0 件の賞賛
返信
1 返信

1,335件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Andy,

    LPC54628 just have the BGA180 package

https://www.nxp.com/docs/en/fact-sheet/LPC546XXFAMFS.pdf 

If you want to use QFP208, you can consider LPC54618, but the core clock is 180Mhz, not 220Mhz.

Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信