LPC54628 (GUI tools suggestion) - reg.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54628 (GUI tools suggestion) - reg.

1,189 Views
PriyeshSah
Contributor I

For MCU LPC54628. We would like to know what GUI tools you would suggest to use. I see that emwin, embedded wizard... Etc are some options. It would be great if you can suggest the best one. 

Thanks in advance. 

0 Kudos
Reply
1 Reply

1,125 Views
soledad
NXP Employee
NXP Employee

Hi, 

You need to evaluate the tools in order to determinate which is the best option for you.

The MCUXpresso SDK is pre-integrated with the SEGGER emWin GUIBuilder, and I suggest to use the SDK for MCU LPC54628.

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply