LPC54628 (GUI tools suggestion) - reg.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54628 (GUI tools suggestion) - reg.

1,224件の閲覧回数
PriyeshSah
Contributor I

For MCU LPC54628. We would like to know what GUI tools you would suggest to use. I see that emwin, embedded wizard... Etc are some options. It would be great if you can suggest the best one. 

Thanks in advance. 

0 件の賞賛
返信
1 返信

1,160件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

You need to evaluate the tools in order to determinate which is the best option for you.

The MCUXpresso SDK is pre-integrated with the SEGGER emWin GUIBuilder, and I suggest to use the SDK for MCU LPC54628.

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信