LPC54628 5v tolerant?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54628 5v tolerant?

2,193件の閲覧回数
mspenard603
Contributor IV

Hi All,

  Does the LPC54628 have 5v tolerant IO?

Looking at the line-card, and while some LPCs explicitly state 5v tolerant IO the LPC54000 doesn't say either way.

https://www.nxp.com/docs/en/product-selector-guide/LPCMICROLNCD.pdf 

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,056件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hi Mike, 

Could you please post your new question in the i.MX RT space (link), so the correct person can help you out.

Thank you!

Sabina

0 件の賞賛
返信

2,056件の閲覧回数
mspenard603
Contributor IV

Thank you sir.

I've been trying to verify this with the iMX RT1062 as well. I've read through all the available docs here, but can't seem to find a mention:

i.MX RT1060 MCU/Applications Crossover Processor | Arm® Cortex®-M7 @600 MHz, 1MB SRAM | NXP 

0 件の賞賛
返信

2,056件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello!

 

In reference to the manual the I/O pins are typically 5V tolerant. The footnotes for Table 4, specify the different configurations for different  pins in the LPC546XX datasheet. In addition you can refer to page 83 of the same document for the limiting values on the pins. It is always recommended to work slightly below the limits.

For specific pin configurations which can allow for 5V, please refer to the LPC546XX datasheet:

https://www.nxp.com/docs/en/data-sheet/LPC546XX.pdf

 

For general information regarding these pins functions, refer to the LPC546XX manual:

https://www.nxp.com/webapp/Download?colCode=UM10912

 

 

Hope this helps!

0 件の賞賛
返信