LPC54618J512 RMII Interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54618J512 RMII Interface

Jump to solution
1,534 Views
andrew_sig
Contributor I
Hi! I'm trying to implement Ethernet communication between an LCP54618J512 and a LAN8720 module [https://www.ebay.com/itm/233331877929].
I previously tested with the LPCXpresso development board, which uses a 25 MHz XTAL, and everything works perfectly. I also tested with the LAN8720 module and an ESP32, overriding the 50 MHz clock output and generating the required 50 MHz signal in RMII mode using an ESP32 terminal.
Is it possible to use an LPC54618 terminal to generate the 50 MHz signal? The terminals I'm currently using are:

LAN8720

PHY (RMII)

LPC54618

TXD0

ENET_TXD0

PIO4_19 (14)

TXD1

ENET_TXD1

PIO4_20 (18)

TX_EN

ENET_TX_EN

PIO4_27 (85)

RXD0

ENET_RXD0

PIO4_23 (42)

RXD1

ENET_RXD1

PIO4_24 (67)

CRS_DV

ENET_RX_DV

PIO5_1 (126)

MDC

ENET_MDC

PIO5_3 (129)

MDIO

ENET_MDIO

PIO5_4 (135)

nINT/RETCLK

RMII_REF_CLK

PIO4_14 (194)

nRST

Reset PHY (optional)

PIO4_16 (203)

 

If I need to use the 50 MHz generated from the LAN8720 module clock, is there any sample code I can use?
Thanks'
Labels (2)
0 Kudos
Reply
1 Solution
1,502 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @andrew_sig 

Is it possible to use an LPC54618 terminal to generate the 50 MHz signal?

Harry_Zhang_0-1752226102419.png

 

I think yes, you are correct: the P3_12 pin (CLKOUT) can be configured to output a clock signal, and it can be used to provide a 50 MHz reference clock to the LAN8720 PHY for RMII operation.

Is there any sample code I can use?

Currently, there is no related sample code.

BR

Harry

View solution in original post

0 Kudos
Reply
2 Replies
1,488 Views
andrew_sig
Contributor I
Hi! Thanks for your response. I believe PIO3_12 can be used as indicated in the LPCXpresso 54608 user manual.
I'll try a code implementation using MCUXpresso Config Tool, and see what results it gives

 

0 Kudos
Reply
1,503 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @andrew_sig 

Is it possible to use an LPC54618 terminal to generate the 50 MHz signal?

Harry_Zhang_0-1752226102419.png

 

I think yes, you are correct: the P3_12 pin (CLKOUT) can be configured to output a clock signal, and it can be used to provide a 50 MHz reference clock to the LAN8720 PHY for RMII operation.

Is there any sample code I can use?

Currently, there is no related sample code.

BR

Harry

0 Kudos
Reply