LPC54618 IBIS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54618 IBIS

2,666 Views
EngHuiPeng
NXP Employee
NXP Employee

Customer Samina is asking for the LPC54618 as I can only locate the LPC5410X ibis. Appreciate your advice.

Regards,

Audrey

0 Kudos
Reply
3 Replies

2,582 Views
soledad
NXP Employee
NXP Employee

Hi, 

Unfortunately, we don't have IBIS models available for the LPC546xx family. 

Sorry for any inconvenience that may cause. 

Have a nice day!

Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,582 Views
EngHuiPeng
NXP Employee
NXP Employee

Soledad,

Can customer use the model from any of the same family like LPC5410x?

Thanks.

Regards,

Audrey

0 Kudos
Reply

2,582 Views
soledad
NXP Employee
NXP Employee

Hi, 

The resistance, inductance, capacitance model will be different from other LPC devices such as 5410x, even the same family different package.

 

Have a nice day!

Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply