LPC54616 Unique ID

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54616 Unique ID

Jump to solution
2,598 Views
travis_scott
Contributor II

Hi all,

I am trying to read the 128 bit unique ID from the LPC54616. There is an IAP routine, but other answers suggest it can be read from a flash address directly. Can anyone confirm this address?

Thanks

Labels (1)
0 Kudos
Reply
1 Solution
2,522 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Travis Scott 

We can read LPC546xx UID from address from 0x01000100 to 0x01000103.

See user manual, I highlight the code as below:

pastedImage_1.png


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,523 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Travis Scott 

We can read LPC546xx UID from address from 0x01000100 to 0x01000103.

See user manual, I highlight the code as below:

pastedImage_1.png


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,522 Views
travis_scott
Contributor II

Thanks very much, I was using rev 2.1 of the user manual which didn't have this. Perfect

0 Kudos
Reply
2,522 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

Have a nice day,

Jun  Zhang

0 Kudos
Reply