LPC54616 SCTimer input

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC54616 SCTimer input

跳至解决方案
2,982 次查看
wangyanjun
Contributor II

As described in the manual, Tx_OUT0 can be used as SCTimer input.

But what is the Tx_OUT0? Is CTimer's match output or others?

0 项奖励
回复
1 解答
2,960 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, YanJun,

Thank you for the feedback. If the CTimer is used to counts external clock, and you want to test the external signal clock frequency, you can use the CTimer as a divider, the CTimer outputting clock signal can function as a capture signal for the SCT, with the capture function, the SCT can test the external signal frequency.

BR

XiangJun Rong

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,972 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, YanJun,

As the following Fig shows, the Tx_OUT0 can be an input signal for the SCT module, the signal can function as capture signal, which can generate event with programmable rising/falling edges, if you enable an interrupt, the event can trigger an interrupt. With the capture function, user can test the width of the signal..

Hope it can help you

BR

XiangJun Rong

 

xiangjun_rong_0-1610435435898.png

 

0 项奖励
回复
2,967 次查看
wangyanjun
Contributor II

Thank you for your reply.

I found the answer from MCUxpresso Config Tools. The Tx_OUT0 is the CTimer's match channel 0 output.

0 项奖励
回复
2,961 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, YanJun,

Thank you for the feedback. If the CTimer is used to counts external clock, and you want to test the external signal clock frequency, you can use the CTimer as a divider, the CTimer outputting clock signal can function as a capture signal for the SCT, with the capture function, the SCT can test the external signal frequency.

BR

XiangJun Rong

 

0 项奖励
回复