LPC5460x USB composite MSC to SPIFI flash example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC5460x USB composite MSC to SPIFI flash example

ソリューションへジャンプ
3,227件の閲覧回数
cybaluke
Contributor III

Hi everybody, I am just starting a project using LPC5460x  and  MCUXPRESSO IDE, I need to have a USB composite interface to manage a USB virtual com port to control the main embedded app from a host PC and a USB MassStorageClass interface to download some data files (they are a couple of .bin files for other micro/dsp on the board and other files of raw data used by the main app) from the host PC to the SPIFI flash on board (MX25L12835FM2I-10G). Note: all the embedded firmware functions will run in internal LPC flash.

Could you suggest me the right example for LPC5460x to starting from to code a USB Mass Storage Class that can write data files from the host PC to SPIFI flash and can you suggest how (if it is possible) to port it in a composite VirtualCom and Mass Storage Class?

Best regards

ラベル(5)
0 件の賞賛
返信
1 解決策
2,940件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Luke

MCUXpresso SDK software also provides below USB-MSC example for your reference:

pastedImage_1.png

Please find them with below path:

C:\nxp\SDK_2.3.1_LPCXpresso54608\boards\lpcxpresso54608\usb_examples

You also could download the MCUXpresso SDK USB stack help document from MCUXpresso SDK config website.

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,940件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Customer could refer [usb_device_composite_cdc_msc] demo as the start project.

MCUXpresso SDK software package also provides SPIFI example code with below path:

C:\nxp\SDK_2.3.1_LPCXpresso54608\boards\lpcxpresso54608\driver_examples\spifi

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,940件の閲覧回数
cybaluke
Contributor III

Thanks Mike for your help.

SPIFI is not the real problem for me but I'm a USB-stack beginner so I started from lpcxpresso54608_dev_composite_cdc_msc_lite_bm example (as you suggested) but I don't know very well UFI standard and in general USB stack, so it's difficult for me to understand when e where (in what handlers) manage the incoming and outcoming datas from the host PC. 

I was looking for a "USB-MSC for dummy" example or some references to understand where insert in the USB handlers my callbacks for SPIFI reading and writing functions.

best regards

luke

0 件の賞賛
返信
2,941件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Luke

MCUXpresso SDK software also provides below USB-MSC example for your reference:

pastedImage_1.png

Please find them with below path:

C:\nxp\SDK_2.3.1_LPCXpresso54608\boards\lpcxpresso54608\usb_examples

You also could download the MCUXpresso SDK USB stack help document from MCUXpresso SDK config website.

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,940件の閲覧回数
cybaluke
Contributor III

Thanks Mike for the help, I think "usb_device_msc_sdcard_lite_bm" could be a good starting point for my work, SDK.2.4.0 misled me, it doesn't has the same samples of the SDK.2.3.1...

0 件の賞賛
返信