LPC54608 flashiap

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54608 flashiap

2,460 Views
実奥山
Contributor II

I wrote the MAC address in flash using flashiap.

Below was made based on a sample of NXP.

MAC address  was included in page_buf, and copied this in a flash.

But I don't understand the way to read this data from a flash.

Please tell me the way to read data of a flash using flashiap.

    /* Program sector */
    for (i = 0; i < (FSL_FEATURE_SYSCON_FLASH_SECTOR_SIZE_BYTES / FSL_FEATURE_SYSCON_FLASH_PAGE_SIZE_BYTES); i++)
    {
        FLASHIAP_PrepareSectorForWrite(7, 7);
        FLASHIAP_CopyRamToFlash(
            //FSL_FEATURE_SYSCON_FLASH_SECTOR_SIZE_BYTES + (i * FSL_FEATURE_SYSCON_FLASH_PAGE_SIZE_BYTES), &page_buf[0],
            0x38000 + (i * FSL_FEATURE_SYSCON_FLASH_PAGE_SIZE_BYTES), &page_buf[0],
            FSL_FEATURE_SYSCON_FLASH_PAGE_SIZE_BYTES, SystemCoreClock);
    }

Labels (1)
0 Kudos
Reply
2 Replies

2,099 Views
実奥山
Contributor II

I can  read data  by below(flashdata).

const unsigned char flashdata= *(unsigned char *)0x038000;

I use LPC54608J512 and this device have 512K flash(0 to 15 sectors).

But I can not access 8 to 15 sectors.

Please teach me how to access 8 to 15 sectors.

0 Kudos
Reply

2,099 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Customer,

    Yes, if you want to read the flash data, just read that address's data is OK.

    You said, you can't access 8 to 15 sectors, please check, do you control the correct address?

pastedImage_1.png


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply