LPC54608 external cystal configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54608 external cystal configuration

2,246 Views
prathap_ponnuch
Contributor I

Hi All,

I am using LPC54608 mcu for our project.

In this 25MHz crystal is there.

Internal 12MHz FRO running successfully with this board.

But we need to configure 25Mhz external crystal oscillator how to configure?

How to set with external oscillator?

Thanks in advance.

Regards,

prathap

Labels (1)
0 Kudos
Reply
3 Replies

2,206 Views
prathap_ponnuch
Contributor I

Hi Jun Zhang,

Thanks for replay and Sorry for the delay.

pastedImage_1.png

Here cant able to see clock config setting.Where we need to go and set?

Thanks in advance.

Regards,

prathap

0 Kudos
Reply

2,206 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Follow below steps to go to clock config tool

pastedImage_1.png

pastedImage_2.png

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,206 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi prathap ponnuchamy 

You can easily config clock with Clock Config tool integrated inside MCUXpresso IDE. 

By default, fro_12M is used as PLL input to provide system clock. 

if you want to use external clock as pll input, just config SYSPLLCLKSEL to select clk_in as source. see below.

pastedImage_3.png

your external clock is 25M, just config sys osc as 25Mhz, you need make sure PLL output frequency range is between 275MHz-550MHz.

after configuration, don't forget update code:

pastedImage_4.png


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply