LPC54608 Usart Interrupt Example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54608 Usart Interrupt Example

2,678件の閲覧回数
mpazzi
Contributor III

Hello,

I have a question in relation about the Usart Interrupt LPC54608 example, that I re-write down here:

pastedImage_1.png

First question: Why I collect data from the usart also if I have an error (kUSART_RxError) ?

Second question: I haven't found any point where the status of kUSART_RxError is deleted in the code?

If I well understand, on the relative manual it is sayed that must be reset by software.

pastedImage_2.png

Where I'm wronging ?

Thanks a lot for help.

Marco

ラベル(1)
0 件の賞賛
返信
1 返信

2,351件の閲覧回数
Ray_V
Contributor V

First let me say that I do not have the example and I am only replying from my experience without actually looking at the code

First question: Why I collect data from the usart also if I have an error (kUSART_RxError) ?

If you received this error the FIFO is full. the data needs to be pulled out of the FIFO or it will keep getting this error when new data arrives 

Second question: I haven't found any point where the status of kUSART_RxError is deleted in the code?

DEMO_USART_IRQHandler() is not invoked directly as an interrupt handler. It is called by the actual USART interrupt handler, my guess is that it is cleared in the actual interrupt handler (e.g. USART0_IRQHandler)