LPC54608 UART TX open drain or not?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54608 UART TX open drain or not?

1,013 Views
実奥山
Contributor II

I'd like to use the pin named P0_30-ISP_FC0_TXD(A2) as a USART transmitter.

Is this pin an open drain pin by a default mode?

If this pin is an open drain pin, I have to put pull-up resistor.

I don't want to put pull-up resistor.

Please tell me whether pull-up resistor is needed.

In the same way.
When also using D3,P12 pin as a USART transmitter, please tell me whether pull-up resistor is needed.

Labels (1)
0 Kudos
Reply
1 Reply

898 Views
soledad
NXP Employee
NXP Employee

Hi,

This is a stardard I/O pin.The default configuration for standard I/O pins is Z mode. The weak MOS devices provide a drive capability equivalent to pull-up and pull-down resistors.

The below figure shows the possible pin modes for standard I/O pins:

• Digital output driver: enabled/disabled.

• Digital input: Pull-up enabled/disabled.

• Digital input: Pull-down enabled/disabled.

• Digital input: Repeater mode enabled/disabled.

• Z mode; High impedance (no cross-bar currents for floating inputs).

pastedImage_1.png


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply