LPC54608 SPIFI RAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54608 SPIFI RAM

1,405件の閲覧回数
A_M
Contributor III

Hello,
we wanted to use LPC54608 but we need more RAM and we can't use SDRAM(EMC), we need the other pin functions.

That's why we want to connect the external RAM is through SPIFI.
At startup the firmware configures the SPIFI to command mode. Copies the data from the USB or SPI to the SPIFI Ram and executes it from there.

Are there any problems with this configuration?

ラベル(2)
0 件の賞賛
返信
1 返信

1,381件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

LPC540xx can support SPIFI boot ( Boot from QSPI NOR flash device connected to SPIFI interface. ), but LPC54608 doesn't support.

The available boot source for LPC546xx is as below:

ZhangJennie_0-1653290462189.pngZhangJennie_0-1653290462189.png

User needs to access SPIFI device from internal Flash.

 

Best Regards

Jun Zhang

 

 

0 件の賞賛
返信