LPC54608 SPIFI RAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC54608 SPIFI RAM

1,434 次查看
A_M
Contributor III

Hello,
we wanted to use LPC54608 but we need more RAM and we can't use SDRAM(EMC), we need the other pin functions.

That's why we want to connect the external RAM is through SPIFI.
At startup the firmware configures the SPIFI to command mode. Copies the data from the USB or SPI to the SPIFI Ram and executes it from there.

Are there any problems with this configuration?

标签 (2)
0 项奖励
回复
1 回复

1,410 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

LPC540xx can support SPIFI boot ( Boot from QSPI NOR flash device connected to SPIFI interface. ), but LPC54608 doesn't support.

The available boot source for LPC546xx is as below:

ZhangJennie_0-1653290462189.png

User needs to access SPIFI device from internal Flash.

 

Best Regards

Jun Zhang

 

 

0 项奖励
回复