LPC54608 Reset switch issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54608 Reset switch issues

7,293件の閲覧回数
germano
Contributor II

Hi! I'm working with a custom board based on a LPC54608.

Generally everything works fine, however, sometimes when you press the reset button. The microcontroller remains frozen and does not start, and I need to disconnect the power and reconnect it to correct the problem.


My reset circuit is shown in the figure below.
reset.png

Is it necessary to consider something else to restet the microcontroller?
ラベル(1)
0 件の賞賛
返信
7 返答(返信)

7,029件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi germano,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
to be honest, according to the schematic, it's hard to find the cause of the phenomenon.
I'd like to know the mean of 'microcontroller remains frozen and does not start', does the external crystal Y1 can start up successful?
Maybe you should confirm whether the MCU enter the ISP mode.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

7,029件の閲覧回数
microcris
Contributor III

In my case, the  MCU enters the ISP mode.

It "randomly switches" between ISP0, ISP1 and ISP2. Since those pins are connected to EMC bus, It depends from whom is low at the reset moment. 

And, again in my case, it happens more often when I preform two consecutive resets because I start a full sdram consistency scan immediately after a reset.

Thank you for pointing out the possibility of entering in ISP without external command.

0 件の賞賛
返信

7,029件の閲覧回数
germano
Contributor II

Hi jeremyzhou,

'microcontroller remains frozen and does not start' means that the flash program doesn' start.

The cristyal is working fine, at the same frequency always.

On ISP select pins I copied the circuit of LPCXpresso54608, but I don't know how to chek if the MCU is on ISP Mode or not.

pastedImage_2.png

Anyway, is there any way to ensure that the MCU does not initialize in ISP mode?

Edit: I found that the issue is more frecuent when the reset switch is pressed while MCU is writing on SDRAM

0 件の賞賛
返信

7,029件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi germano,

Thanks for your reply.
According to your attachment, I find that the PIO0_4 (ISP_0), PIO0_5 (ISP_1) and PIO0_6 (ISP_2) will be used as the EMC data pins, to eliminate the potential interference of the status of these data pins, add two pull-up resistors to PIO0_5 and PIO0_6, just did with the PIO0_4, or assert the CRP_ISP_DISABLE_PIN bit to disable the ability to enter ISP mode using the ISP pin.

pastedImage_1.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

7,029件の閲覧回数
germano
Contributor II

Thank you!

The pull up resistors didn't work, but I fix the issue by writing OTP to disable ISP Mode.

0 件の賞賛
返信

7,029件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi germano,

Thanks for your reply.
Glad to hear that the issue is resolved:smileyhappy:.


Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

7,029件の閲覧回数
microcris
Contributor III

I have the same problem with a LPC54628.

It seems to happen when two resets are issued in a very short time. 

lpc_reset.png

0 件の賞賛
返信