LPC54608 PIO3_10 pull up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54608 PIO3_10 pull up

1,735件の閲覧回数
実奥山
Contributor II

When resetting,is GPIO pin PIO3_10(port3 bito10) in the pull up state?

Please refer to attachment.

It isn'tsetting pull up by  the data seat.

It's setting  pull up by the user's manual.

Which is right?

I checked it by an evaluation board.

 The port is high when open state.

So I think Pull up is enable.

ラベル(1)
0 件の賞賛
返信
1 返信

1,658件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

By default this pin has internal pull-up enabled. Thank you for your feedback I will check this with the documentation team.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信