I have configured in the following manner:
1. Cleared ADC, VREFP, VDDA, TS, ANA & wait for 20us
2. ADC clock enable, AHBCLKCTRL0.
3. Clear the ADC0 peripheral reset using the PRESETCTRL0 register
4. set temperature channel in INSEL
5. Enable ADC & set clock to 15MHz using CLKDIV in ctrl register
5. Set Synchronous mode , 12-bit resolution, BYPASS = 0, TSAMP = 0
6. then configures sequence A in SEQA_CTRL, CHANNELS = 1, TRIGGER = 0, TRIGPOL = 0, SYNCBYPASS = 0, BURST = 0, SINGLESTEP = 0, LOWPRIO = 0, MODE = 0, SEQA_ENA = 1
7. SET CALIB = 1 & waited till CALIB = 0
8. then started conversion by START bit, read result
but result is same everytime & DATA VALID is not setting.