LPC54608 CLKOUT 25MHz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54608 CLKOUT 25MHz

1,477件の閲覧回数
実奥山
Contributor II

I use OM13092 board.

Can I take out 25MHz from CLKOUT?

The following clock can be chosen in CLKOUTSEL regster.

main_clk, clk_in,fro_hf,pll_clk etc.

Which clock should I choose?

Can FRO be set as 96MHz or 48MHz?

Is it main_clk to be equivalent to FRO?

I think I have to choose a clock bigger than 25MHz by CLKOUTSEL.

Please tell me how to make 25MHz.

ラベル(1)
0 件の賞賛
返信
1 返信

1,347件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi 実 奥山,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I'd highly recommend you to use the MCUXpresso Config Tool to configure the clock, as the tool provides a graphical interaction interface to help the developer to do it.

MCUXpresso Config Tools|Software Development for NXP Microcontrollers (MCUs)|NXP 
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信