LPC54606 usage with KSZ8091RNB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC54606 usage with KSZ8091RNB

Jump to solution
2,710 Views
rene_benvenuti
Contributor II

Hi,

We are plannig to develop a board using 100-pin LPC54606 and add ethernet communication with KSZ8091RNB RMII phy.

We already have a similar product using LPC4078 processor, however, I notice that RMII pins are different on these processors. For LPC4078 we use the CRS_DV MAC pin, witch is missing on LPC546x. We also tried out to use RX_DV pin for this function on LPC4078 without success.

It is possible to use LPC546x in RMII mode? We are not sure about using the RX_DV pin for the same role of CRS_DV.

Best regards,

Renê

Labels (2)
1 Solution
2,609 Views
diego_charles
NXP TechSupport
NXP TechSupport

Yes is possible to use LPC546x in RMII mode.

As you could check, in our schematic for the LPCxpresso546x, 

the LAN8720A-CP PHY, which supports the RMII  MAC interface, is implemented among the LPC54608 RMII interface.

 

Please note that in the schematic design the ENET_RX_DV pin of the LPC546x is connected to the CRS_DV pin of the PHY.

Best regards, Diego. 

View solution in original post

2 Replies
2,610 Views
diego_charles
NXP TechSupport
NXP TechSupport

Yes is possible to use LPC546x in RMII mode.

As you could check, in our schematic for the LPCxpresso546x, 

the LAN8720A-CP PHY, which supports the RMII  MAC interface, is implemented among the LPC54608 RMII interface.

 

Please note that in the schematic design the ENET_RX_DV pin of the LPC546x is connected to the CRS_DV pin of the PHY.

Best regards, Diego. 

2,609 Views
rene_benvenuti
Contributor II

Thanks for your help, Diego!

We will try it out on KSZ8091 PHY.

0 Kudos
Reply