LPC54606 usage with KSZ8091RNB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54606 usage with KSZ8091RNB

ソリューションへジャンプ
2,008件の閲覧回数
rene_benvenuti
Contributor II

Hi,

We are plannig to develop a board using 100-pin LPC54606 and add ethernet communication with KSZ8091RNB RMII phy.

We already have a similar product using LPC4078 processor, however, I notice that RMII pins are different on these processors. For LPC4078 we use the CRS_DV MAC pin, witch is missing on LPC546x. We also tried out to use RX_DV pin for this function on LPC4078 without success.

It is possible to use LPC546x in RMII mode? We are not sure about using the RX_DV pin for the same role of CRS_DV.

Best regards,

Renê

ラベル(2)
1 解決策
1,907件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Yes is possible to use LPC546x in RMII mode.

As you could check, in our schematic for the LPCxpresso546x, 

the LAN8720A-CP PHY, which supports the RMII  MAC interface, is implemented among the LPC54608 RMII interface.

 

Please note that in the schematic design the ENET_RX_DV pin of the LPC546x is connected to the CRS_DV pin of the PHY.

Best regards, Diego. 

元の投稿で解決策を見る

2 返答(返信)
1,908件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Yes is possible to use LPC546x in RMII mode.

As you could check, in our schematic for the LPCxpresso546x, 

the LAN8720A-CP PHY, which supports the RMII  MAC interface, is implemented among the LPC54608 RMII interface.

 

Please note that in the schematic design the ENET_RX_DV pin of the LPC546x is connected to the CRS_DV pin of the PHY.

Best regards, Diego. 

1,907件の閲覧回数
rene_benvenuti
Contributor II

Thanks for your help, Diego!

We will try it out on KSZ8091 PHY.

0 件の賞賛
返信