LPC54606 in QFP100 package and SDRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54606 in QFP100 package and SDRAM

ソリューションへジャンプ
2,333件の閲覧回数
carstengroen
Senior Contributor II

The LPC54606 comes (also) in a QFP100 package. It is shown in the datasheet that it supports 8/16 bit EMC interface. It has support for port 0 and port 1 so most of the EMC (for SDRAM) signals are there.

However, the EMC_A[14] are only located on P3.25 which is not available on the 100 pin package. EMC_A[13] and EMC_A[14] are connected to BA0 and BA1 on a 16 bit SDRAM device. Is there some different connections to be used on the 100 pin package, or is it not possible to support 16 bit SDRAM on this package ?

ラベル(2)
0 件の賞賛
返信
1 解決策
1,895件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Carsten Groen,

The EMC supports 8/16 bit data bus on BGA100 package, you can learn the more information about the SDRAM interface to LPC546xx external memory controller via the application note.

http://www.nxp.com/docs/en/nxp/application-notes/AN12026.pdf 

TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,895件の閲覧回数
carstengroen
Senior Contributor II

Could really use a hint regarding this....

0 件の賞賛
返信
1,896件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Carsten Groen,

The EMC supports 8/16 bit data bus on BGA100 package, you can learn the more information about the SDRAM interface to LPC546xx external memory controller via the application note.

http://www.nxp.com/docs/en/nxp/application-notes/AN12026.pdf 

TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,895件の閲覧回数
carstengroen
Senior Contributor II

Thanks a lot Jeremy!

I was not aware of that application note (I see it went online 2 days before my original question :smileywink:), the text:

pastedImage_1.png

explains it perfectly, thanks :smileyhappy:

0 件の賞賛
返信