LPC54606 firmware.bin filesize

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC54606 firmware.bin filesize

1,568件の閲覧回数
vijo
Contributor III

Hi,

when booting to USB Mass Storage Device, the size of the firmware.bin file is 516K = 512K + 4K

The size of the internal CPU flash is 512K.

Where does the 4K come from ?

Regards

Viggo

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,371件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Viggo,

Please refer the following community post: https://community.nxp.com/message/1023684 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 件の賞賛
返信